AXIS#.HOME.CREEPFACTOR

Description

AXIS#.HOME.CREEPFACTOR is the percentage of the homing speed (AXIS#.HOME.V) used when searching for the feedback’s index or limit switch. AXIS#.HOME.CREEPFACTOR is only used in home modes 1, 2, 3, 6 and 10.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

This content is not applicable to KAS.

Type

Read/Write

Units

%

Range

1 to 100

Default Value

50

Data Type

Integer

See Also

AXIS#.HOME.V, AXIS#.HOME.MODE

Stored in Non-Volatile Memory

Yes

Fieldbus Information

CANopen Over EtherCAT (COE)

Name

Index

SubIndex

Data Type

Access

PDO Mappable

AXIS1.HOME.CREEPFACTOR

5008h

2h

Unsigned32

Read/Write

No

AXIS2.HOME.CREEPFACTOR

5108h

2h

Unsigned32

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

AXIS#.HOME.CREEPFACTOR

6105

17D9

Unsigned32

Read/Write

PROFINET

Parameter

PNU

Data Type

Access

AXIS#.HOME.CREEPFACTOR

6105

Unsigned32
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
AXIS1.HOME.CREEPFACTOR

5008h

0bh

Unsigned32

-

-

Read/Write

No

AXIS2.HOME.CREEPFACTOR

5108h

0bh

Unsigned32

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.HOME.CREEPFACTOR

6105

17D9

Unsigned32

Read/Write

-

AXIS2.HOME.CREEPFACTOR

71641

117D

Unsigned32

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.HOME.CREEPFACTOR

6105

Unsigned32

Read/Write

-

Related Topics

Homing